Cancel
Showing results for 
Search instead for 
Did you mean: 

TC 9132 to TC 11.2.3 upgrade fails

Creator
Creator

Hi All

 

TC 9132 to TC 11.2.3 upgrade fails at post schema adds , anyone came across these issues ? any inputs will help !

Generating exception: Sat Sep 30 19:07:13 EDT 2017
An error occurred during execution. Stack trace follows...
com.teamcenter.install.tceng.base.DatabaseSteps.upgradeDatabase(DatabaseSteps.java:1038)
com.teamcenter.install.tceng.base.Foundation.install(Foundation.java:201)
com.teamcenter.install.tceng.base.Foundation.upgrade(Foundation.java:1142)
sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
java.lang.reflect.Method.invoke(Method.java:483)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:209)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:135)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1423)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1361)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1265)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1179)
com.teamcenter.install.tem.struct.TcFeature.upgrade(TcFeature.java:1107)
com.teamcenter.install.tem.director.actions.UpgradeAction.execute(UpgradeAction.java:25)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:134)
java.lang.Thread.run(Thread.java:745)
Searching for 'x of y' comment(s)
Adding comment: 67 of 243
Adding comment: 90 of 243
Adding comment: 91 of 243
Adding comment: 92 of 243
Adding comment: 93 of 243
Adding comment: 94 of 243
Adding comment: 95 of 243
Adding comment: 96 of 243
Adding comment: 97 of 243
Adding comment: 98 of 243
Adding comment: 99 of 243
Adding comment: 100 of 243
Adding comment: 101 of 243
Adding comment: 102 of 243
Adding comment: 105 of 243
Adding comment: 106 of 243
Adding comment: 108 of 243
Adding comment: 123 of 243
Flushing comment(s) from the system

3 REPLIES

Re: TC 9132 to TC 11.2.3 upgrade fails

Valued Contributor
Valued Contributor

Unfortunatelly I cannot give you an answer.

But in our case we have updated at first from TC9.x to TC10.x and then to TC11.2.1.

Re: TC 9132 to TC 11.2.3 upgrade fails

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
This is an unusual error but upgrading Tc9.1.3.2 to Tc11.2.3 as a single step is supported. You'll need to review the upgrade logs in TC_ROOT\logs for additional info on the failure. Also look for a shell.err in that dir.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TC 9132 to TC 11.2.3 upgrade fails

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Please check the latest TC_ROOT\install\install*.log to find out the command\utility that is failing. You can then check the corresponding utility log\syslog in TC_ROOT\logs folder to get more details for that failure.