Cancel
Showing results for 
Search instead for 
Did you mean: 

TC_Auto_Checkout

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello Comunity,

 

I have an Issue. In One of our Customers Teamcenter we have set "TC_Auto_Checkout= OFF". As I unterstood, it has to work like this. "User A" checks out a Dataset, he can work, edit, save and when he finished "CheckIn" this Dataset. 

My Problem is when "User A" Checks out a Dataset to reserve it (for example: to work after lunch on this dataset), but doesn't work directly with the Dataset. Now, "User B" is able to cancel the checkout of "User A". 

 

Is this normal? or is there any possibility to change this?

 

Best regards,

 

Youssef

7 REPLIES 7

Re: TC_Auto_Checkout

Siemens Genius Siemens Genius
Siemens Genius

The ability to cancel checkout relate to Access Control, you should to look on Access Control Tree

All the best, Alexey.

Re: TC_Auto_Checkout

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello Alexey,

 

I compared the ACL between old ProdSystem and new ProdSystem. I don't see any change in ACL.

 

It was an Upgrade from Teamcenter 10 (10.1.3.2(20150331.00)) 64-Bit to Teamcenter 11 (11.5.0.3(20180813.00)) 64-bit.

 

Could it be something with the Upgrade? And where would I have to look?

 

Thanks for replying

 

Youssef

Re: TC_Auto_Checkout

Siemens Genius Siemens Genius
Siemens Genius

These users in same group or role? 

All the best, Alexey.

Re: TC_Auto_Checkout

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi ,

 

Firstly you should check the mentioned users are is the same group/role or not ? Because in ACL , i think so, it setted for the having same access to reach datas.

 

Best Regards

Gurkan

Re: TC_Auto_Checkout

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Alexey,

 

thanks for reply.

 

yes they are. But even one of our Experts couldn't handle this. We opened a Call at Siemens and waiting for Response.

 

Best regards,

Youssef

 

Re: TC_Auto_Checkout

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Gurkan,

 

Thanks for your reply, too.

 

As I answered to Alexey, it has to be something with the 11.5 Version. In TC115 it doesn't work as in the older VersionTC9.

 

Best regards,

 

Youssef

Re: TC_Auto_Checkout

Pioneer
Pioneer

Hi.

 

Can somebody please show me the place of the settings where to get this "autocheckout" OFF? Screenshot would be nice, thank you.