Cancel
Showing results for 
Search instead for 
Did you mean: 

TC Client install

Pioneer
Pioneer

Can anyone please explain what I have to do here;

 

*************************************************************************
*************************************************************************
Operation: Install Mode
Config ID: TcRS_Configuration1
Recovery Mode? false
Maintenance Mode? true

Features currently installed
Microsoft Visual C++ Runtimes
Client Communication System
2-tier server configurations
JtUtilities Support
Teamcenter Rich Client 2-tier
NX Foundation/Runtime Server
Features to be added
NX Rich Client Integration
Features to be removed
Microsoft Visual C++ Runtimes
Features to be deprecated
None
*************************************************************************
Loading C:\Siemens\TCPD\2tNX11\install\uninstall.xml
=====================================================
Processing <preuninstall> feature Microsoft Visual C++ Runtimes
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
=====================================================
Processing <uninstall> feature Microsoft Visual C++ Runtimes
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
=====================================================
Processing <postuninstall> feature Microsoft Visual C++ Runtimes
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
Removing tags for 'A0CF69C3A0BC61770EB81BD22667EA52'
Removing tags for 1 features
Cleaning up
***
***Cleaning files
***
Deleting C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Teamcenter 11\Teamcenter 11.lnk
Deleting C:\Users\Public\Desktop\Teamcenter 11.lnk
***
***Cleaning directories
***
Deleting directory C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Teamcenter 11, recurse: false
Deleting directory C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Teamcenter 11
=====================================================
Processing <files> feature NX Rich Client Integration
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
=====================================================
Processing <preinstall> feature NX Rich Client Integration
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
=====================================================
Processing <install> feature NX Rich Client Integration
Time: Wed Apr 13 11:12:00 AEST 2016
=====================================================
Running com.teamcenter.install.tceng.rc.struct.NxRc
Copying file C:\Siemens\TCPD\2tNX11\portal\templates\start_nxmanager.bat.template

Executing ["C:\Program Files\Siemens\NX 10.0\ugii\env_print.exe" -v]
Output from command: "C:\Program Files\Siemens\NX 10.0\ugii\env_print.exe" -v
V28.0.3.5
command_exit=0
Exit Status 0, elapsed time 0:00:00
Copying file C:\Siemens\TCPD\2tNX11\portal\portal.bat
An error occurred during execution. Stack trace follows...
com.teamcenter.install.util.struct.windows.RegistryKey.<init>(RegistryKey.java:170)
com.teamcenter.install.util.struct.windows.RegistryKey.setValue(RegistryKey.java:1164)
com.teamcenter.install.util.struct.windows.RegistryKey.setValue(RegistryKey.java:1183)
com.teamcenter.install.tceng.rc.struct.NxRcWindows.setMIMEType(NxRcWindows.java:24)
com.teamcenter.install.tceng.rc.struct.NxRc.install(NxRc.java:52)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:162)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:128)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1407)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1345)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1245)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1159)
com.teamcenter.install.tem.struct.TcFeature.install(TcFeature.java:1079)
com.teamcenter.install.tem.director.actions.InstallAction.execute(InstallAction.java:29)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:134)
java.lang.Thread.run(Unknown Source)
***
*** CANCELLED
***
=====================================================
Installation interrupted due the following reason:

Processing <install> of feature NX Rich Client Integration failed: com.teamcenter.install.util.struct.windows.Win32Exception: Failed to open 'HKEY_CLASSES_ROOT\MIME\Database\Content Type\application/ugmportal', error 5.: 5
Time: Wed Apr 13 11:12:28 AEST 2016
=====================================================

=====================================================
CommentStore
=====================================================
An internal error occured which has caused processing to stop.
Severity: 1 (Severe)

=====================================================
Copying file C:\Siemens\TCPD\2tNX11\install\configuration.xml

1 REPLY

Re: TC Client install

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Launch TEM with "Run as administrator". In the uninstall above, you don't have write access to the registry. Operating system error 5 means "Access is denied".

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4