Cancel
Showing results for 
Search instead for 
Did you mean: 

TC DATA is web application layer?

Valued Contributor
Valued Contributor

Hi, I have a question. 

We use 4 tier client and I am creating ppt about how to do the backup. In that, I faced one question.

 

TC data and TC root is in web application layer?

Or  they are in client layer?

 

 

Please help me...

3 REPLIES

Re: TC DATA is web application layer?

Phenom
Phenom

Hi @Gimec,

 

Web application layer (or web tier) is a Java based application server which manages communication between 4-tier client and server manager. So neither TC Data nor TC Root are in web app layer.

 

As far as I understood the  architecture concepts: TC_ROOT is in client layer and TC_DATA should be in resource tier.

Re: TC DATA is web application layer?

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
I like to think that TC_DATA is in the application layer (along side server manager) and that TC_ROOT can be in the resource, application, web and clients layers (anywhere TC is installed). There are some exceptions where TC_ROOT may not be in the web layer, like with the J2EE architecture, where only the tc.ear file is deployed (built using INSWEB) or TC_ROOT isn't in the client layer, like with the OTW architecture, where the rich client is built with INSWEB (PORTAL_ROOT). If you install Teamcenter using TEM on a machine then it has a TC_ROOT.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TC DATA is web application layer?

Valued Contributor
Valued Contributor

Thank you so much.