Cancel
Showing results for 
Search instead for 
Did you mean: 

TC Embedded Viewer configuration for PDF

Genius
Genius

Hello,

 

I have a problem with embedded viewer for PDF, in prop defaultViewerConfig.VIEWERCONFIG I add PDF.TCTwoDViewer=PDF_Reference,PDF  but in viewer i got an error "Failed to open document".

 

TC version 10.1.4

SE ST9 + TC 10.1.7
3 REPLIES 3

Re: TC Embedded Viewer configuration for PDF

Legend
Legend

Is Teamcenter visualization installed (embedded)?

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: TC Embedded Viewer configuration for PDF

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

The PDF.TCTwoDViewer recommended for 64bit environments is a TcVis viewer. In order to view a PDF, TcVis Embedded Viewer needs to be installed and have permission for both "opening/viewing" and "Content Copying". Another option is to use Adobe Reader but it will take a bit more configuration to work correctly (see 7429849, 7636778 on GTAC).

 

Don't forget to run %TC_ROOT%\portal\registry\genregxml.bat.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Highlighted

Re: TC Embedded Viewer configuration for PDF

Genius
Genius

Thx for advices. TC Visualisation is not instaled (IT departments maked instalation and forgot do this). Now I set Adobe Reader as deafult viwever and is working properly.

SE ST9 + TC 10.1.7