Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

TC Vis Patch Silent Script

Creator
Creator

Hi,

 

We have TC V1122 in our environment. We need to apply patch 11221 on the existing Visualization installation using silent script. But we could not find silent script for the same .Could anyone help how to perform the patch upgrade using silent script

6 REPLIES 6

Re: TC Vis Patch Silent Script

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is information about automatic or silent installation of TcVis patches in the read-me of the patch, which is available at the same point as the patch exe.

I think you could also run the patch exe from a command prompt with the -? switch or similar to get a usage hint.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: TC Vis Patch Silent Script

Creator
Creator

Hi Pendi, Thanks. I will check the readme and try out the installation

Re: TC Vis Patch Silent Script

Siemens Phenom Siemens Phenom
Siemens Phenom
Use the command line option "-ai": e.g. TcVis_10150_win64.exe -ai

Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: TC Vis Patch Silent Script

Creator
Creator

Thanks all it is working

Re: TC Vis Patch Silent Script

Legend
Legend

you can try msiexec with options too

Re: TC Vis Patch Silent Script

Creator
Creator

Hi,

 

You can create an custom batch file with the necessary details for installation (kill java,cache, etc and run the installer), Before running the installer using batch script manually provide the entry for license server and also about which features needs to be installed and then you can package it using NSIS script.

 

you can later push it via OTW and using custom ICD u can also push it to the users machines