Cancel
Showing results for 
Search instead for 
Did you mean: 

TC property (ootb) is in display name for item active and should be in catia file name too

Experimenter
Experimenter

Hello together,

I created a new customized property "customer" for an item and this property is also set into the display name for the item.  "customer"_itemID_name etc. 

 

When I create a dataset for catia and load it into catia, only the id is visible as part or product number.

 

I can add the revision name with the preference: CATIA_part_file_name_format

But i want to add the "customer" property too, to the part or product number in CATIA. 

So that the name in catia also displays the "customer".

 

Any ideas??

 

 

thanks,

GabB