Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

TC11.4 and NX12 Preview Pics for Pax files @ File New

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Gys,

 

I already looked to the help, https://docs.plm.automation.siemens.com/tdoc/nx/12.0.1/nx_help#uid:index_tcint:id1299958:xid1130165:... but I could not find any help there.

 

I got the issue that my preview pics are not shown when I start the File New Command i don't see my preview pics.

 

How must they be written @pax file or placed to be found? The UGII_Template is set and native it works well. In XML do I need a hardcoded path or how?

 

Maybe you guys have me a hint, and if it was already discussed here please show my i couldn´t find a solution in my searches.

2 REPLIES 2

Re: TC11.4 and NX12 Preview Pics for Pax files @ File New

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Open the parts and save them to generate the preview images. This is a post task to importing the files from a pax and is normal.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TC11.4 and NX12 Preview Pics for Pax files @ File New

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Randy,

 

it wasn´that easy in some points. The problem i had is that i first needed to import the images_preview.qaf file and the dependet txt file for it. Then i editet that text file so it does not look for the drawing or model qaf. 

 

After that i change in NX that the preview is generated automatically. Then it worked

 

thx for the hint, that brought me to it