Cancel
Showing results for 
Search instead for 
Did you mean: 

TC12.0 SOA Client FMS Issue-FileUpload/Download

Hello Team,

 

I am trying to upload/download files using FileManagementUtility Service.

I have defined correct FMS_HOME path also given lib paths in PATH Variable.

 

Capture.JPG

 

Here it says...

 

Could not open FCCJavaClientProxy library (FCCJavaClientProxyv12064 or FCCJavaClientProxyv10064). Make sure FMS_HOME is set properly.
java.lang.UnsatisfiedLinkError: no FCCJavaClientProxyv10064 in java.library.path
at java.lang.ClassLoader.loadLibrary(Unknown Source)
at java.lang.Runtime.loadLibrary0(Unknown Source)

 

I have checked in tccs\lib directory there are files for FCCJavaClientProxyv*****.dll but not with above mentioned version.

 

Where i can find required dll's?

 

Regards,

Ganesh 

4 REPLIES 4

Re: TC12.0 SOA Client FMS Issue-FileUpload/Download

Gears Phenom Gears Phenom
Gears Phenom

@GaneshDasmale - are you running a stand alone TCCS? Or are you running this from a server? I'd try running fccstat to see if you are communicating or not. I'm running TC12.1 but my dll's aren't the same as you have listed. 

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: TC12.0 SOA Client FMS Issue-FileUpload/Download

Thanks for the reply,

 

yeah, i am trying to write a SOA utility, by which i want to upload & download named references.

i need to provide FMS_HOME for it, to communicate FCC and then through it to FSC.

FSC is up n running, FCC is also started.

It is working for TC11.2 but not with TC12.0

 

Re: TC12.0 SOA Client FMS Issue-FileUpload/Download

Legend
Legend

the missing dlls exist in a standalone installation of tccs 11.2

try to install tccs (11.2) and then update it to tccs (12.0)

Re: TC12.0 SOA Client FMS Issue-FileUpload/Download

Legend
Legend

but a TC12.0 SOA Client should not need tccs 11.2 libraries?

Someting wrong with your build of the 12.0 soa client?