Cancel
Showing results for 
Search instead for 
Did you mean: 

TC12 fails to import NX templates

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

I'm having problems importing NX12 templates into TC12. I'm lauching the import utility, it executes and says that the import is successfull, but no templates are actually imported - and also utility terminates suspiciously promptly.

Has anyone had the similar problem before? Are there any Tc logs that I need to have a look at?

 

echo.pngnew problem.png

10 REPLIES 10

Re: TC12 fails to import NX templates

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, did you try to run a command, without the -action key, as in the documentation?
Do you use 2-tier or 4-tier for installation? 4-Tier requires additional environment variables

 

https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help/#uid:index_tcint:id1299958:xid1130165...

 

Re: TC12 fails to import NX templates

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello! Sorry for the late response!

I have a 2-tier environment. I tried running withouth the -action key and it did not seem to make any difference.

Re: TC12 fails to import NX templates

Siemens Legend Siemens Legend
Siemens Legend

it has been a while when I was importing File-New-Templates of NX to Teamcenter.

I never had a problem with opening the NX-CMD-Prompt from the start menu, set TC_ROOT=<your-tc-root-path-here> and TC_DATA=<your-tc-data-path-here>, change directory to %UGII_BASE_DIR%\UGII\templates\sample and run the tcin_template_setup skript with the login arguments (-u=infodba -p=*** -g=dba)...

(I know that the DOCS tell it a bit different...)

Re: TC12 fails to import NX templates

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I have no problem running it either. It is getting the result that I have problem with. :-)

I successfully ran this utility on previous versions of TC, but with this one something is wrong.

Probably faulty installation. I did not do it, so I don't know what options were picked.

Highlighted

Re: TC12 fails to import NX templates

Siemens Legend Siemens Legend
Siemens Legend

within your installation - you can launch NX from Teamcenter?

if not - can you check on the server if the "NX Integration" feature (I hope I spelled it correctly) is enabled/installed?

 

it would be interesting what the tcserver*.syslog and $USERNAME*.syslog (NX-log) say for the import?

Re: TC12 fails to import NX templates

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks for the involvement! My issue has been successfully resolved by GTAC.

Re: TC12 fails to import NX templates

Siemens Legend Siemens Legend
Siemens Legend
can you give as some words what the problem was and how you resolved it?

Re: TC12 fails to import NX templates

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Apparently the problem was spaces in the NX path. Yes, in this day and age!

The solution was to change in tcin_template_setup.bat:

@files = glob( $template_dir . '\*' );
to
@files = glob( "'" . $template_dir . '\*' . "'");

Re: TC12 fails to import NX templates

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I am getting the same issue. I tried the solution mentioned here as well, still it is same.