Cancel
Showing results for 
Search instead for 
Did you mean: 

TCCS with NX Launcher Issue

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello together,

 

we installed a TC Server and in our VM Ware NX Launcher is working fine. If we try now to install tccs on a client to connect to the Vm Ware we allways recive the messsage "Failed to get the TCCS Einvironment: [name] we enterd"

 

Where is the TCCS Environment name defined? We think it is the Servername but evry option we tried, fails.

Servername, DB Name, Instancename, Clientname, fantasyname, evryname fails.

 

How must TCCS be installed that it works? IF we connect in the VM with 2 Tier it works.

 

TC12.1 NX 1851 but we can reproduce it with TC11, TC112 NX 11 NX12 NX 1847

2 REPLIES 2

Re: TCCS with NX Launcher Issue

Siemens Phenom Siemens Phenom
Siemens Phenom
how did you install TCCS on the client?
TCCS won't work for 2-tier, only 4-tier!

Re: TCCS with NX Launcher Issue

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi

 

opps forgot to close the thread. i allready solved it.

 

Fun Fact it works on my machine with a NX Launcher in a tier connection and 4 Tier.

 

Problem was a typo in the path