Cancel
Showing results for 
Search instead for 
Did you mean: 

TCServer Crashes when pool Manager is started

Experimenter
Experimenter

Pool manager crashes with the following information during startup. Launching the pool manager via command line.

 

INFO - NoId - 2018/05/31-06:57:12,615 UTC - LapcyPro12 - TreeCache View: [192.168.2.191:17800|0] [192.168.2.191:17800]
INFO - NoId - 2018/05/31-06:57:12,618 UTC - LapcyPro12 - TreeCache GMS address: 192.168.2.191:17800
tecs>2018/05/31-06:57:13,419 UTC MLD Log init: com.teamcenter.mld version V11000.2.0.41_40_20171020.00 (20171020)
tecs>log.properties found at D:\app\Teamcenter\TC_ROOT\pool_manager\confs\config1\log.properties
WARN - 1 - 2018/05/31-06:57:14,312 UTC - LapcyPro12 - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
tecs>INFO - NoId - 2018/05/31-06:57:15,711 UTC - LapcyPro12 - TECS is not running
INFO - NoId - 2018/05/31-06:57:15,767 UTC - LapcyPro12 - TECS started by ServerManager. Output is written to D:\app\Teamcenter\TC_ROOT\pool_manager\confs\config1\tecs.out
INFO - NoId - 2018/05/31-06:57:15,767 UTC - LapcyPro12 - To terminate TECS, use D:\app\Teamcenter\TC_ROOT\pool_manager\confs\config1\tecsstop
WARN - 1 - 2018/05/31-06:57:16,149 UTC - LapcyPro12 - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
INFO - NoId - 2018/05/31-06:57:17,467 UTC - LapcyPro12 - Server tcserver2@PoolA@13004@LapcyPro12 finished
WARN - NoId - 2018/05/31-06:57:17,484 UTC - LapcyPro12 - Information about server tcserver2@PoolA@13004@LapcyPro12 discarded. Process 11344 does not exist.
WARN - 1 - 2018/05/31-06:57:18,912 UTC - LapcyPro12 - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
INFO - NoId - 2018/05/31-06:57:18,966 UTC - LapcyPro12 - Server tcserver3@PoolA@13004@LapcyPro12 finished
WARN - NoId - 2018/05/31-06:57:18,968 UTC - LapcyPro12 - Information about server tcserver3@PoolA@13004@LapcyPro12 discarded. Process 11964 does not exist.
WARN - 1 - 2018/05/31-06:57:20,138 UTC - LapcyPro12 - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
INFO - NoId - 2018/05/31-06:57:20,172 UTC - LapcyPro12 - Server tcserver4@PoolA@13004@LapcyPro12 finished
WARN - NoId - 2018/05/31-06:57:20,172 UTC - LapcyPro12 - Information about server tcserver4@PoolA@13004@LapcyPro12 discarded. Process 10720 does not exist.
WARN - 1 - 2018/05/31-06:57:36,075 UTC - LapcyPro12 - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
INFO - NoId - 2018/05/31-06:57:36,119 UTC - LapcyPro12 - Server tcserver5@PoolA@13004@LapcyPro12 published
ERROR - Failed to connect to the Teamcenter server.

 

The Tcserver processes are started and getting terminated with the following statements in syslog.

 

***********************TC Server Log*********************************************

 

NFO - 2018/05/31-06:58:03.991 UTC - LapcyPro12.13224 - The Transient Volume Root Directory is C:\Temp\transientVolume_infodba - Teamcenter.Organization.sa at D:\workdir\tc11301_a01_win64\src\core\sa\filetickets.cxx(1264)
ERROR - 2018/05/31-06:58:03.991 UTC - Thread-13224: - The start line and headers have already been committed to the request. Cannot send again.- Teamcenter.SOA.Tctp
FATAL - 2018/05/31-06:58:03.991 UTC - LapcyPro12.13224 - FATAL EXCEPTION: Top level exception handler invoked. - Teamcenter.SOA.tcserver_itk_main at D:\workdir\tc11301_a01_win64\src\server\tcgateway\main\tcserver_itk_main.cxx(486)
POM enquiries statistics: created 32, undone 0, deleted 18, queried 31

 

************************TC Server Log*******************************************

 

Can someone throw some insight on the above issue ?

 

Thank you.

 

 

 

 

8 REPLIES 8

Re: TCServer Crashes when pool Manager is started

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I haven't seen that error before. Usually a TcPipeException is related to a timeout and not "Accept failed". The timeout is controlled by receive_timeout in TctpConfig.xml. Basically, the tcserver process is trying to talk to the Server Manager process when this "Accept failed" message occurs.

Can you tell us about your server/situation:
What OS are you running?
What Teamcenter version are you running?
What Java version are you running?
Is the CPU load heavy?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TCServer Crashes when pool Manager is started

Experimenter
Experimenter

Hello Randy,

 

It looks Strange, I have not modified any of those configuration files with respect to timeout. However, the tcserver processes are getting started and terminated abruptly within a small time frame(5 to 10 seconds).

 

This is the syslog Message:

Teamcenter.Organization.sa at D:\workdir\tc11301_a01_win64\src\core\sa\filetickets.cxx(1264)
INFO - 2018/06/06-07:33:56.615 UTC - LapcyPro12.13920 - Teamcenter Server is ready. - Teamcenter.SOA.tcserver_itk_main
ERROR - 2018/06/06-07:33:56.870 UTC - Thread-13920: - Connect error: 0- Teamcenter.SOA.Tctp
ERROR - 2018/06/06-07:33:56.870 UTC - Thread-13920: - TctpServer failed to accept a TcPipe on the named pipe tcserver3@PoolA@7012@LapcyPro12. acceptPipe failed- Teamcenter.SOA.Tctp

 

Please find the details below.

What OS are you running?

Windows 10 PRO
What Teamcenter version are you running?

Teamcenter 11 (11.3.0.1_a01_1(20171020.00)) 64-bit

What Java version are you running?

JRE Version: 1.8.0_121 64-bit
Is the CPU load heavy?

No, it seems normal and I have around 5GB of free RAM space available. Total RAM Capacity is 12GB.

 

Does this issue has anything to do with the OS

Highlighted

Re: TCServer Crashes when pool Manager is started

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

The pool manager is designed as a server process and not a client so Win10 is likely the culprit. Why install directly on Win10 when you have Hyper-V for free on Win10? My recommendation is to install the Hyper-V option and create a WS2012 vm that holds the DB, .NET Server Manager and IIS for the .NET WebTier. Then run your VM and RAC 4t on Win10. I do this myself.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: TCServer Crashes when pool Manager is started

Experimenter
Experimenter
Hello Randy,

Thank you for the information. I shall try the above option and Share the results :)

Re: TCServer Crashes when pool Manager is started

Experimenter
Experimenter

Hey, Do you find any solution for the above mentioned problem?

Re: TCServer Crashes when pool Manager is started

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello ,

Did you find this solution for this error ?

we too got the same error. Can you share the deatils, if it solved.

 

Thanks

 

Re: TCServer Crashes when pool Manager is started

Creator
Creator

Hi Expret,

 

Did anyone resolved this issue. i also got the error while starting pool manager.

 

-------------------------------------------------------
GMS: address is 137.55.172.205:17800
-------------------------------------------------------
INFO - NoId - 2019/05/14-10:34:56,773 UTC - DESKTOP-QA547IC - TreeCache View: [137.55.172.205:17800|0] [137.55.172.205:17800]
INFO - NoId - 2019/05/14-10:34:56,774 UTC - DESKTOP-QA547IC - TreeCache GMS address: 137.55.172.205:17800
tecs>2019/05/14-10:34:57,226 UTC MLD Log init: com.teamcenter.mld version V11000.2.0.60_20181019.00 (20181021)
tecs>log.properties found at C:\apps\Siemens\Teamcenter11\pool_manager\confs\config1\log.properties
tecs>INFO - NoId - 2019/05/14-10:34:59,283 UTC - DESKTOP-QA547IC - TECS is not running
INFO - NoId - 2019/05/14-10:34:59,348 UTC - DESKTOP-QA547IC - TECS started by ServerManager. Output is written to C:\apps\Siemens\Teamcenter11\pool_manager\confs\config1\tecs.out
INFO - NoId - 2019/05/14-10:34:59,349 UTC - DESKTOP-QA547IC - To terminate TECS, use C:\apps\Siemens\Teamcenter11\pool_manager\confs\config1\tecsstop
WARN - 1 - 2019/05/14-10:35:05,681 UTC - DESKTOP-QA547IC - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
WARN - 1 - 2019/05/14-10:35:05,707 UTC - DESKTOP-QA547IC - Error occurred in ServerPipe.
com.teamcenter.io.TcPipeException: Accept failed
at com.teamcenter.io.ServerTcPipe.acceptPipe(Native Method)
at com.teamcenter.io.ServerTcPipe.accept(Unknown Source)
at com.teamcenter.tctp.server.TctpServer$1.run(Unknown Source)
INFO - NoId - 2019/05/14-10:35:05,768 UTC - DESKTOP-QA547IC - Server tcserver2@PoolA@11992@DESKTOP-QA547IC published
INFO - NoId - 2019/05/14-10:35:05,768 UTC - DESKTOP-QA547IC - Server tcserver1@PoolA@11992@DESKTOP-QA547IC published
ERROR - Failed to connect to the Teamcenter server.
TcPipeException: Read failed.
ERROR - Failed to connect to the Teamcenter server.
TcPipeException: Read failed.
ERROR - Failed to connect to the Teamcenter server. Read failed.
ERROR - Failed to connect to the Teamcenter server. Read failed.
ERROR - The request XML:
<?xml version="1.0" encoding="UTF-8"?>
<GetValidMetricsInput xmlns:ns2="http://teamcenter.com/Schemas/Soa/2006-03/Base" xmlns="http://fnd0.com/Schemas/Internal/DebugMonitor/2011-06/DebugMonitor"/>
ERROR - The request XML:
<?xml version="1.0" encoding="UTF-8"?>
<GetValidMetricsInput xmlns:ns2="http://teamcenter.com/Schemas/Soa/2006-03/Base" xmlns="http://fnd0.com/Schemas/Internal/DebugMonitor/2011-06/DebugMonitor"/>
ERROR - The response XML:
Empty
ERROR - The response XML:
Empty
ERROR - NoId - 2019/05/14-10:35:07,378 UTC - DESKTOP-QA547IC - com.teamcenter.schemas.soa._2006_03.exceptions.InternalServerException: Failed to connect to the Teamcenter server. Read failed. com.teamcenter.jeti.serversubpoolmanager.ServerHealthMetrics

Re: TCServer Crashes when pool Manager is started

Experimenter
Experimenter

PLease try reverting any windows update that got pushed recently on to your machine. That should resolve the issue. And stop Automatic updates feature if possible. Hope this helps. Thanks.