Cancel
Showing results for 
Search instead for 
Did you mean: 

TCTYPE_ask_child_primary_types sample code

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

 

Anyone aware of sample code that involves TCTYPE_ask_child_primary_types.

 

Thanks,

Roy

5 REPLIES 5

Re: TCTYPE_ask_child_primary_types sample code

Siemens Creator Siemens Creator
Siemens Creator

Hey Roy, what is the concrete question?

How to use it or what is the purpose?

Re: TCTYPE_ask_child_primary_types sample code

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

 

Hi Oliver -

 

RE:  " How to use it or what is the purpose?   "

 

How to use it.  

 

For example,  with TCTYPE_list_properties,  I use PROPDESC functions to access/display the meta data that is in the returned tag(by TCTYPE_list_properties),  as follows -

==================================================================

status = TCTYPE_list_properties(itemTypeTag, &n_properties, &property_descriptors);

 status = PROPDESC_ask_name(property_descriptors[ii], &prop_name);

status = PROPDESC_ask_display_name(property_descriptors[ii], &disp_name);
 printf("PROPERTY NAME -> [%-30s] ", prop_name);

printf("PROPERTY DISPLAY NAME -> [%s]\n", disp_name);

=====================================================================

 

What do I use with TCTYPE_ask_child_primary_types, to access/display the meta data that is returned from TCTYPE_ask_child_primary_types ?

 

Thanks,

Roy

 

Re: TCTYPE_ask_child_primary_types sample code

Siemens Creator Siemens Creator
Siemens Creator

Sorry, still not clear for me since you said you want to know how to use it but then later asking 'what do I use with it?' which sounds like asking for the purpose ;)

 

Purpose:
TCTYPE_ask_child_primary_types might be used if you want to retrieve all the primary TYPE TAGs (!not objects!)  of the context (secondary) object which might be connected via any relation.

 

How to use it:

1. Get the type_tag (which represents any POM type in BMIDE/system) of the context object by using:
TCTYPE_ask_object_type(obj_tag, tag_t *type_tag)

2. Use the type_tag as input for the function TCTYPE_ask_child_primary_types:
TCTYPE_ask_child_primary_types(type_tag, int* number_of_child_types, tag_t** child_types);

3. The return primary types you may want to combine with your code snippet example:
TCTYPE_list_properties(child_types[i], &n_properties, &property_descriptors);
...

 

Re: TCTYPE_ask_child_primary_types sample code

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Yes,  I understand.  Thanks !

Re: TCTYPE_ask_child_primary_types sample code

Siemens Creator Siemens Creator
Siemens Creator

you're welcome :-)