Cancel
Showing results for 
Search instead for 
Did you mean: 

Tc 11 help files

Gears Phenom Gears Phenom
Gears Phenom

In NX11, the help files can be pulled directly from the Siemens PLM website, eliminating the need for a local install, and the java issues we have all fought.

 

Can this be done with Tc 11 as well?  avoiding the local document server, etc?

-Dave
NX 11 | Teamcenter 11 | Windows 10
2 REPLIES

Re: Tc 11 help files

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I haven't tried it yet but it should be possible. You will need internet access at all times.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Tc 11 help files

Siemens Phenom Siemens Phenom
Siemens Phenom

I entered the SPLM server in the site specific file and it worked fine.

 

# Help - web server or if direct, file://
portalHelpWebServer=https://docs.plm.automation.siemens.com/tdoc/tc/
# Portal Help Files path
portalHelpPage=11.2.2/help/

 

Nice idea as it is pretty flexible and no installation is needed but one needs the webkey.