Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Teamcenter 10 installation Error

Siemens Phenom Siemens Phenom
Siemens Phenom

Do you have Windows 7 Enterprise?

Highlighted

Re: Teamcenter 10 installation Error

Builder
Builder

@xtof,

 

I am trying to install it on Windows 7 64 bit machine.I am not using any enterprise version.

Re: Teamcenter 10 installation Error

Siemens Phenom Siemens Phenom
Siemens Phenom
The supported os for Teamcenter 10 are Win 7 SP1 x64 Pro & Ent. Do you have Pro? I do not know if the problem has something to do with the supported os but I would not recommend to install on unsupported os anyway.
xtof

Re: Teamcenter 10 installation Error

Builder
Builder

@xtof,

 

Recommended OS is required. But it should met client side requirements right.

Re: Teamcenter 10 installation Error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
According to Google, your error is common on Windows when the Microsoft Visual C++ Redistributables are wrong, .NET Framework is not supported or DirectX needs reinstalled. I know people that have had trouble with the .NET Framework version and the solution was to uninstall .NET 4.5 then install .NET 3.5 and .NET 4.5 over top. The .NET Framework installation is order specific. In other words, your problems not with Teamcenter (just a symptom).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 10 installation Error

Creator
Creator

make sure you run your TEM.bat as Administrator, or could you tell me what is TEM_SEENVA ? thanks.

Re: Teamcenter 10 installation Error

Builder
Builder

@LarryPhil,

 

I don,t know much about this.But it is aa environment variable.