Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 11 Login error

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I am investigating the attached TC-11 login error.

 

Appreciate any information.

 

 

21 REPLIES 21

Re: Teamcenter 11 Login error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The Tc preferences that define the http string are likely wrong. The 7001 port is the default for WebLogic and I think you installed JBoss which has a default of 8080.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11 Login error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi @RoyHutchens ,

Randy is right , it will be caused by the communication failed with the main server. Firstly you can try to set the port as default 8080 then you will check the telnet <servername> port and maybe you check port according to the that link.

https://www.howtogeek.com/howto/28609/how-can-i-tell-what-is-listening-on-a-tcpip-port-in-windows/

Maybe you can check the firewall or antivirus program , which can protect to reach main server by using the port 7001 or 8080.

 

Best Regards

Gurkan

 

Re: Teamcenter 11 Login error

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I greped on my Teamcenter root,  and found one hit for '7001' at -

 

C:\Teamcenter\Tc11.2.0a_win64\tc\ssrs_adapters\ssasDataProvider\app.config

 

I backed up app.config to 'app.config.backup',  and changed -

 

<add key="Port" value="7001"/>

 

to

 

<add key="Port" value="8080"/>

 

I rebooted my machine to make sure any relative variable would be reset.

 

However,  I have the same error,  and it continues to indicate port 7001.

 

Is there a specific place where I would change the port ?   Registry ?

 

Thanks,

Roy

 

 

Re: Teamcenter 11 Login error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Teamcenter preferences are stored in the Database. Can you run a Tc command window? If so then try this:
Create a text file containing "WEB_default_site_server" and call it "PrefList.txt" (in C:\Temp).
In Tc cmd run:
cd /d C:\Temp
preferences_manager -u=infodba -p=infodba -g=dba -mode=export -scope=SITE -file=PrefList.txt -out_file=C:\Temp\PrefsFix.xml

Note: No spaces in file names nor path.

Then modify PrefsFix.xml (or attach it here) then run:
preferences_manager -u=infodba -p=infodba -g=dba -mode=import -scope=SITE -file=C:\Temp\PrefsFix.xml -action=OVERRIDE


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11 Login error

Siemens Genius Siemens Genius
Siemens Genius

Roy,

please share with us:

.....\portal\plugins\configuration_##000.1.0\client_specific.properties

All the best, Alexey.

Re: Teamcenter 11 Login error

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

I presume the 'Tc command window' would be an option under the TC menu ?

or

Would I open an MS command window and run something to set the environment ?

 

Attached are my TC-11 menu command options.

Re: Teamcenter 11 Login error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The wording may be tripping you up. The picture you show is for Start. Whereas, we are talking about TC_ROOT\tc_menu\*.bat for starting a Tc command window.

Or you can build the Tc command window on your own by opening a command window on the server (cmd) and running:
set TC_ROOT=full_path_to_tcroot
set TC_DATA=full_path_to_tcdata
call %TC_DATA%\tc_profilevars.bat

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11 Login error

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

 

I have two properties files under my TC root -

 

 

C:\Teamcenter\Tc11.2.0a_win64\install\expressregistrykeys.properties

 

C:\Teamcenter\Tc11.2.0a_win64\install\temui.properties

Re: Teamcenter 11 Login error

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Nope. TC_ROOT\tc_menu is a directory. If you don't see it then you're not looking at the server where Foundation is installed.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4