Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Creator
Creator

Does anybody have experience with Teamcenter 11.2 .NET Web tier and Windows Server 2016? My problem is in connection with the Internet Information Service (IIS). Windows Server 2016 comes with IIS 10. I can not install the Web tier because "IIS 7.0 or above version is required", however I enabled the proper Windows features (all except WebDav and FTP).

 

I would appreciate any ideas.

7 REPLIES 7

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Creator
Creator

I may have found a solution:

 

  1. Open Regedit > HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\InetStp
  2. Edit "MajorVersion" and set the "DECIMAL" value to 8
  3. Hit F5 while in Regedit
  4. Install TC Web Tier
  5. Change the "MajorVersion" back to "DECIMAL" value of 10
  6. Hit F5 while in Regedit
  7. Close Regedit

The installion was succesful. Of course further testing is required...

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

As Windows Server 2016 is not supported by Teamcenter it is not a good idea to run TC in this environment.

xtof

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

May I know if this issue has been solved and if Win Server 2016 works well with TC 11?

 

We will be implementing and thinks of a server version that won't have any issue with TC 11.

Hope I can get an input from you. Thanks!

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Creator
Creator

Hi,

Make a quick search for the Teamcenter Combatibility Matrix! According to it with the new version (Tc11.3) ISS 10 was certified with Windows Server 2016.

Microsoft IIS

7.5 on Window 2008 R2

8.5 on Windows 2012 R2

At Tc11.3 - 10 was certified with Windows Server 2016

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Legend
Legend

Is this issue got fixed for you?

 

It will be helpful if you share us the details

 

Thanks,

Rafa

Regards
Rafa

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

Yes, I was able to install TcRS 11.3 on WinSer 2016 by following scr's instructions:

 

  1. Open Regedit > HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\InetStp
  2. Edit "MajorVersion" and set the "DECIMAL" value to 8
  3. Hit F5 while in Regedit
  4. Install TC Web Tier
  5. Change the "MajorVersion" back to "DECIMAL" value of 10
  6. Hit F5 while in Regedit
  7. Close Regedit

Regards,

Lyka

Re: Teamcenter 11 Web tier and Windows Server 2016 (IIS 10)?

Thanks, It worked!