Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 2T launch Error

Pioneer
Pioneer

Hi experts,

While launching 2T tc, I am getting error as below (copied from TAO window).

 

 

Checking for currently running TAO ImR services...
No running TAO ImR services found...
1 file(s) copied.
Starting ImplRepo service...
ImR_Adapter::init with default servant
server TcServer1 is_alive = 0
report_ior <IOR:010000002900000049444c3a496d706c656d656e746174696f6e5265706f7369746f72792f4c6f636174
6f723a312e3000000000010000000000000090000000010102000a0000003132372e302e302e310024064400000014010f00
4e5550000000210000000001000000526f6f74504f4100496d706c5265706f5f53657276696365000000000001000000496d
706c5265706f5f53657276696365020000000000000008000000016d3800004f41540100000018000000016d380001000100
01000000010001050901010000000000>
Implementation Repository: Running
Ping Interval : 10000ms
Startup Timeout : 60s
Persistence : C:\Users\girish\Teamcenter\TAO\tcserver.xml
Multicast : Disabled
Debug : 2
ReadOnly : False

Starting ImR Activator...
(5992|2472) EXCEPTION, ImR_Activator_i::init_with_orb
system exception, ID 'IDL:omg.org/CORBA/INTERNAL:1.0'
TAO exception, minor code = 0 (endpoint initialization failure in Acceptor Registry; unspecified err
no), completed = NO

(5992|2472) EXCEPTION, System Exception
system exception, ID 'IDL:omg.org/CORBA/INTERNAL:1.0'
TAO exception, minor code = 0 (endpoint initialization failure in Acceptor Registry; unspecified err
no), completed = NO

 

 

Any one know about this thing..

 

Thank you.

5 REPLIES

Re: Teamcenter 2T launch Error

Phenom
Phenom

Good afternoon,

1) Check your host file, it should not contain records with the same ip addresses

2) Check that port 1572 is not occupied by another application

3) Check that you do not have TAO running in your processes. It can be run from under another user.

Re: Teamcenter 2T launch Error

Pioneer
Pioneer

@ArthurRM 

 

Checked all the 3 points, all are fine..

But still getting same error:smileyhappy:... 

Re: Teamcenter 2T launch Error

Phenom
Phenom

Is your host file empty or something written in it?

Re: Teamcenter 2T launch Error

Pioneer
Pioneer

@ArthurRM

 

Here is the host file,

please look into this..

 

Thanks.

Re: Teamcenter 2T launch Error

Phenom
Phenom

Good afternoon,

Your file hosts are typical and there are no errors in it. It is necessary to think what else can be the reason