Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter EngineeringUtilityException:POM002

Legend
Legend
Hello Experts,
 
I'm trying to upgrade teamcenter 10.1.7.1 to  11.3 on Windows server 2016 standard
 
Version: SQL server 2012
SPLMLicenseServer_v8.2.5, Teamcenter 11 license file
 
new license file has "INCREMENT teamcenter_admin ugslmd 11.0 permanent 2 SUPERSEDE \"
 
But I got this exception
 
Teamcenter EngineeringUtilityException:POM002
 
 

 

An error has occurred during the operation.  Review the problem description and suggested actions.  If a failure requires some input, the fields will be displayed below.  Click the following log file to some technical information which may be useful in troubleshooting the issue.
Engineering Utility Failure
EngineeringUtilityException: POM002
Description
One of the Teamcenter utilities has failed.
Additional Information
The command returned a value of 1
 
When I checked the install log I see
 
ifail (515209) The operation failed due to an unexpected Database Management System error.
 
Regards
Rafa
2 REPLIES 2

Re: Teamcenter EngineeringUtilityException:POM002

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Have you customized the database? Regen is failing because of a database error...
ODBC error. SQLSTATE: 42S22 Native error: 207
Message: [Microsoft][ODBC SQL Server Driver][SQL Server]Invalid column name 'aspace_uid'.

You should confirm this column with GTAC before continuing.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter EngineeringUtilityException:POM002

Legend
Legend

Hi Randy,

We did not customized the Database, just restored from the backup.

I have raised an IR on this issue, GTAC said that  "“ASPACE_UID” was added in 11.x "

 

And Siemens Dev team is looking into it now

Regards
Rafa