06-16-2017 06:26 PM
I'm having difficulties with a new TC install, unable to connect it up with NX. Looking for help, struggling with the documentation. When I try to launch NX 11.0 in managed mode (I launch it with "C:\Program Files\Siemens\NX 11.0\NXBIN\ugraf.exe" -nx -pim=yes"), I get the following error:
I'm running a 2-tier installation of Teamcenter (10.1.7). I don't understand where or how to point NX to the proper locations. Any help would be greatly appreciated! This is what I installed on my client:
Solved! Go to Solution.
06-17-2017 09:52 AM
The common work-flow is to first start the Teamcenter rich client and then start NX from within it.
To run NX without the rich client, you need to use %UGII_BASE_DIR%\UGMANAGER\ugmanager.bat to start NX in managed mode.
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0 | TcVis 11.4
Employees of the customers, together we are strong
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
06-19-2017 12:46 PM
Thanks. I had kind of figured this out, but it's not super clear. To anyone else looking, from within Teamcenter you launch NX from the File Menu (File->Open in NX). If you don't see that option from the File menu, Go to Edit->Options and under the "NX" option you can set a flag to show the option to launch NX from the File Menu. Don't know why it's not automatically turned on.
06-20-2017 08:11 AM
A bit more info on launching managed NX without the Tc rich client: