Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Performance very low during NX Clone

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Folks,

 

i got an issue i could not find any solution. Situation: Teamcenter 10 and NX9 also Teamcenter 11 and NX11 Customized. In NX we got an PTS Activated part and we put it into an empty part. The PTS is used as clone part. ( The PTS has 3 Parts to clone, 8 to retain) We recive times between 2 Minutes and 9 Minutes. Every operation another time result.

 

If i do it in a OOTB environment i got constant times of 50 seconds with the same part. If i do it native it works also fine, so i guess it is an teamcenter issue.

 

We tested the network and the servers, all fine, they are bored because of nearly nothing to do. So i guess it is the datamodel / customization ( not done by us)

 

any ideas what i can test and look else? 

 

2 REPLIES
Highlighted

Re: Teamcenter Performance very low during NX Clone

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Set these debugging variables in tc_profilevars:

 

set TC_JOURNAL=FULL
set TC_SQL_DEBUG=bJT

 

In a 4-tier environment you have to restart the pool manager, then use JournalWorkbench to review the resulting journal files.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Teamcenter Performance very low during NX Clone

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hi, thx fot the hint and sorry for late response.

i used the tool and find out attribute mapping . but i deactivated it and it still need a lot of time :-)

But thx