Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Rapid Start 10.1.6 - no Online Doku?

Builder
Builder

Hello,

 

I have installed now Teamcenter Rapid Start 10. First TcRS10.1.0 - only Corporate Server, RichClient and BMIDE. Then I have Updated to 10.1.6 und Patched to 10.1.6.1.

Now I going on to install all the Features I need. One of it should be the Online Doku. In the Base-Version of TcRS10.1.0 I found it in the list of features:

 

TcRS10.1.0-OnlineDocu.jpg

But if I would liek to install it now in TcRS10.1.6.1, I did´nt find it anymore. How can I install it?

 

Michael

 

 

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX11.0.2, NX12.0.2
Development: Batch and VB Testing: NX(1847, 1851, 1872)
1 REPLY 1

Re: Teamcenter Rapid Start 10.1.6 - no Online Doku?

Genius
Genius

There are significant changes to online help concept after TcRs 10.1..

 

Installing online help requires separate documentation server..

 

Please see below for some details - (will require GTAC account to see this)

 

https://docs.plm.automation.siemens.com/tdoc/tc/10.1.4/help/#uid:index_whats_new:xid999016:xid104746...