Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Visualization does not show Help - Error 500

Builder
Builder

Hello I installed TcVis 11.2 and its Onlinehelp (PLM Dokumentation Server based). I can start TcVis. When I then will start the Onlinehelp I get this error:

Onlinehelp-Error.jpg

 

The Installation is on Windows Server 2012R2 with JAVA 8u101 (JDK and JRE)

Windows Firewall is OFF, UAC is completely OFF, the Server is in the trustable sites list.

Is it ab problem with the newest Java Version?

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX11.0.2, NX12.0.2
Development: Batch and VB Testing: NX(1847, 1851, 1872)
4 REPLIES 4

Re: Teamcenter Visualization does not show Help - Error 500

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure to install the latest release of the SPLM Docu Server available from the GTAC download page, which is v2.0

The release shipping with Teamcenter is v1.0 and is not working with Java 8u101.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Teamcenter Visualization does not show Help - Error 500

Builder
Builder

Hi Mr. Pendl,

 

I have deinstalled the complete Documentation and DocumentationServer. Now I have installed the new DocumentationServer 2.0 wich is using the new Port 8282. Then I have reinstalled the TcVis OnlineHelp (german-Version) and reconfigured TcVis to the new Port 8282 (old server uses 8181).

When I start OnlineHelp fron TcVis now I get another error:

URL: http://tcnxserv2:8282/data_services/resources/tcv/11.2.2/help/graphics/nonLocalized/collection_startups/tdocExtWeb_visview_base_start.htm

HTTP ERROR: 503

Problem accessing /data_services/resources/tcv/11.2.2/help/graphics/nonLocalized/collection_startups/tdocExtWeb_visview_base_start.htm. Reason:

    Service Unavailable

 

Powered by Jetty://

 

 

Sorry, I would like to put in a new JPG but the link "insert Photo" gets me every time on your reply.

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX11.0.2, NX12.0.2
Development: Batch and VB Testing: NX(1847, 1851, 1872)

Re: Teamcenter Visualization does not show Help - Error 500

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There was no need to remove the previous installation, the in-place update would have just succeeded.

Make sure to revert the port to the old one or you will have to change that port on every client.

I would have restarted the system after removing the doc server, since I think there was still something pointing to the old installation.

You will have to read the installation docs on how to change the port successfully.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
Highlighted

Re: Teamcenter Visualization does not show Help - Error 500

Builder
Builder

Hi Mr. Pendl,

 

I have forgotten to start the Server new after the installation of the new Documentation Server. Now it works.

 

Thank you

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX11.0.2, NX12.0.2
Development: Batch and VB Testing: NX(1847, 1851, 1872)