Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter run error

Experimenter
Experimenter

Hey,

When I try to run Teamcenter 10.0 I get a java error code 13.

as showen in the attached file.

1 REPLY 1

Re: Teamcenter run error

Experimenter
Experimenter

Hi,

 

Check what Java version you have installed on the client.

 

If you run a Tier 4 Client, it's easiest to have Java JRE 7 installed.

 

This since Java JRE 8 creates a different folder structure than Java JRE 7.

JRE 7 is always located in a folder called "C:\Program Files\Java\jre7".

And your Environmental Variable JRE_HOME is pointing to that folder.

But, JRE 8 is different, since it adds the complete name of the current version and update e.g. (C:\Program Files\Java\jre1.8.0_25)

And this change for each update...

 

It is possible to run Java JRE 8 on T4 clients, but it require that JRE_HOME is pointing at the correct JRE 8 folder.

 

I have solved this by running a script before TC (portal.bat) is launched on the clients.

The script check in the registry where the current Java version is installed (java_home). Then I match that towards JRE_HOME. If there is a missmatch, it will update JRE_HOME with the value from java_home and then give the user a message, that he/she needs to start Teamcenter again due to this update. If everything matches, it will launch portal.bat.

 

Hope this helps  ;-)

 

Best Regards

Tobbe