Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter server crash after a short power outage

Experimenter
Experimenter

Hi,

 

We had a short power outage and all client machines restarted automatically.

After that, all the client machines do not have any problem in loggin to Teamcenter.

However, two of the client machines are giving the attached error message.

 

"Initialization failure

 

Teamcenter integration for NX initialize failure

The server returned and internal server error

Teamcenter server failed to respond; system exception, ID 'IDL:omg.org/CORBA/COMM_FAILURE;1.0'

TAO exception, minor code = 6 (failed to recv request response; ENOENT)., completed = MAybe

 

This is most likely the rsult of a crash of the Teamcenter server, or the teamcenter server encountering an unrecoverable error. please check the teamcenter server syslog for more details.

The application will terminate."

3 REPLIES 3

Re: Teamcenter server crash after a short power outage

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
If you question is what to do then I'd suggest restarting them.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter server crash after a short power outage

Experimenter
Experimenter

Thanks for your time and response.

 

Should I restart the Teamcenter Services from the server?

 

 

 

Re: Teamcenter server crash after a short power outage

Experimenter
Experimenter

the issue is resolved after deleting the user:\local temp files.