Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter silent Installation

Siemens Creator Siemens Creator
Siemens Creator

While installing teamcenter on linux machine using silent script I am getting following error

"SEVERE: Error in getting HostName: java.net.UnknownHostException: 1069151-uat-tcserver: 1069151-uat-tcserver: Temporary failure in name resolution"

Is there any wrong in hostname?

1 REPLY

Re: Teamcenter silent Installation

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Is there any wrong in hostname? Depends...
On Linux the max length of hostname is 64 chars (63+null) while Windows still has a 15 char limit due to NetBIOS in some cases. Further, Java doesn't like the dash ("-") and replaces it with an underscore ("-"). My recommendation is to use the lowest common denominator of 15 chars with no special chars. On Linux, if there was a problem with hostname then it should fall back to using localhost which I don't see in your error?
https://community.spiceworks.com/topic/402891-hostname-conventions-vs-netbios-vs-dns

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4