Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter start with Multiple windows User

Pioneer
Pioneer

Hi the community, :smileyhappy:

 

Situation:

Windows User: Paul

--> Open Windows, start Teamcenter and lock Windows Sesssion

 

Windows User: Sandra

--> See Paul is already connected, open her Windows Session, Start Teamcenter -->IMPOSSIBLE

Question:

How can I configure to can be start 2 times Teamcenter with 2 differents Windows account ?

 

Thank you for your help

 

Best Regards

PLM Consultant / Switzerland
10 REPLIES 10

Re: Teamcenter start with Multiple windows User

Phenom
Phenom

Are you using 2 Tier or 4 Tier?

 

I can run multiple sessions of TC in a single windows session in 4 Tier, and I can run multiple sessions of TC in different windows sessions. Im using TC11.2 and windows 10.

 

I cant test with 2 tier.  If you are using 2 tier, and its not possible, then maybe try a bat file that kills Teamcenter and JAVA processes for all users maybe?

 

Just an idea.

Richard Bennett

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Teamcenter start with Multiple windows User

Pioneer
Pioneer

Hi Richard,

 

4Tier client.

 

I can also run multiple TC session in a single windows session.


I cannot start multiple TC session from multiple windows session.

 

Do you know how I can parameter this? The idea is really to lost nothing from the both connection.

 

Thank you

PLM Consultant / Switzerland
Highlighted

Re: Teamcenter start with Multiple windows User

Phenom
Phenom

What happens when you try and run Teamcenter in a diffrent windows session?  Do you get an error message?

 

Richard

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Teamcenter start with Multiple windows User

Pioneer
Pioneer

No error message in the second connection... Teamcenter start on loop.

 

By the past, I've this kind of error (see printscreen)

PLM Consultant / Switzerland

Re: Teamcenter start with Multiple windows User

Phenom
Phenom

Have you tried fccstat - restart? Not sure how it will effect the other session, but you could test.

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Teamcenter start with Multiple windows User

Legend
Legend

Re: Teamcenter start with Multiple windows User

Phenom
Phenom

I havent got this set on my pc...

Richard

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk

Re: Teamcenter start with Multiple windows User

Experimenter
Experimenter

You need to create windows system variable "FMS_WINDOWS_MULTIUSER" with value "true".   

Re: Teamcenter start with Multiple windows User

Pioneer
Pioneer

Hi Vit_konarik,

 

with your solution, I can start Teamcenter into a multiple_session but...

 

Session 1:

        Windows User: Paul

        Teamcenter User: Paul

 

Session 2:

       Windows User: Robert

       Teamcneter User: Robert

 

But... In the session 2, you see the session of Paul.

 

Problem with pipe or/and fmsmaster

 

PLM Consultant / Switzerland