Cancel
Showing results for 
Search instead for 
Did you mean: 

Templates for NX integration with custome Item Types

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

How to add templates for NX with different Item types? I.e. Modelling template for "Item" and for "CAD" item types?

Where should I modify preferences/files to property create and import this templates, because I. I can only see a Item templates and others are invisible in creating new item menu in NX with TC integration.

 

 

Best regards

Bernard Pacula,
CAMdivision Sp. z o.o.
Consultant PLM/System Architect
1 REPLY

Re: Templates for NX integration with custome Item Types

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

NX Templates are imported into Teamcenter using the program NX_BASE_DIR\UGII\templates\tcin_template_setup.bat or tcin_cam_template_setup.bat.

The script will load the appropriate nxdm_*.pax files. Edit nxdm_model_templates.pax to add a section at the bottom that contains your Item types. The ItemType tag is your custom Item type. The Filename tag uses the DB name format:

@DB/<ItemID>/<RevID>

Do the same in any of the other PAX files like nxdm_ugs_drawing_templates.pax or nxdm_ugs_sheet_templates.pax. After editing the PAX files then run the appropriate TCIN batch script to import them. Open a Teamcenter command window, change to the template directory and run the script as an admin.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4