Cancel
Showing results for 
Search instead for 
Did you mean: 

Transferring a structure from PROD to Test environment

Pioneer
Pioneer

Which is the best way to update a structure from PROD to a DEV/test environment? The structure exists in DEV/Test environment but is not the latest as teh database has not been cloned from prod for sometime.

 

Is plmxml the best way? If so which transfer mode to be used? If there is any other way, please suggest.

 

Regards,

RS

3 REPLIES

Re: Transferring a structure from PROD to Test environment

Legend
Legend

Hello,

 

I would suggest to delete the structure in your DEV Environment completely. Then do a plmxml import.

Which tranfermode to be used really depends on the structure contents and what you need from PROD to DEV.

ConfiguredDataExportDefault transfer mode would be sufficient for most use cases or scenarios.

 

Regards

Mahendra

Re: Transferring a structure from PROD to Test environment

Siemens Phenom Siemens Phenom
Siemens Phenom

I do it this way: https://docs.plm.automation.siemens.com/tdoc/tc/11.3/help/#uid:xid1256823:index_plm00094:xid733528

 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Transferring a structure from PROD to Test environment

Pioneer
Pioneer

Thanks Mahendra and Larry. I will check it and come back in case of any queries.

 

Regards,
Rajesh