Cancel
Showing results for 
Search instead for 
Did you mean: 

TransientVolume_infodba :Server cashes and Client

Valued Contributor
Valued Contributor

When I installe the corporation server, I set Generate server cache and Generate Client cache in Fundation panel. But I don't know what is Server cache and what is Client cache?

What kind of informations does each of chase have?

 

 

This points is writen in PDF file called  Installation on Windows Servers Guide at 7-10.

But I don't know what is that.

 

 

 

3 REPLIES

Re: TransientVolume_infodba :Server cashes and Client

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The Client Meta Cache stores static data in a structured manner. Changes to preference values and other static data result in the cache becoming out-of-date and will need to have the cache refreshed. The ClientCache can be found in infodba's Home folder. Cases where the cache should be updated are after a site preference change or an update to batch LOV's.

 

If you are ever in doubt, the cache can be regenerated using the following commands...

generate_client_meta_cache -u=infodba -p=infodba -g=dba
generate_metadata_cache -u=infodba -p=infodba -g=dba -force
generate_client_meta_cache -u=infodba -p=infodba -g=dba -t generate all

These and other utilities are explained in the Utilities Guide.

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: TransientVolume_infodba :Server cashes and Client

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

 

do you now if we can do a " generate_client_meta_cahe" when users are connected in the production database?

 

Thanks

Re: TransientVolume_infodba :Server cashes and Client

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Yes, you can. You may need to restart any warm servers so that they reflect the latest cache or users may get an error message until either Server Manager is restarted or you cycle through all the old warm servers.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2