Cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to create a report in TC 9

Trying to create a report in TC 9 but when I get to the Stylesheet selection I don't see any style sheets to select from. What am I missing?

5 REPLIES 5

Re: Trying to create a report in TC 9

Genius
Genius

Is this a custom query or OOTB ? if this is a custom query, you will have to create a custom stylesheet,import and assign it to the query. On assignment, it will appear to select when you try to generate a report using report builder.

 

reports.JPG

 

 

Hope this helps !!

Cheers.

 

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Trying to create a report in TC 9

Under the report stylesheets I don't have any reports to select from. How do I get to select the one I want to use.

 

 steve.png

Re: Trying to create a report in TC 9

Genius
Genius

I can see many stylesheets when i select the Source as the "Office Template".

reports.JPG

 

I have had the Teamcenter Client for Microsoft office feature installed on my 4 Tier RAC's OTW. Guess that's the reason i am able to see these style sheets.

 

 

You could import the excelsheet into teamcenter as the excel template and then try selecting it.

template.JPG

 

 

template.1JPG.JPG

 

Hope this helps !

Cheers.

 

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Trying to create a report in TC 9

I have imported the excelsheet template into teamcenter and I still don't get anything

Re: Trying to create a report in TC 9

Genius
Genius

Save your XSLX template in XSLT format and import the dataset. You should be able to select it.

 

For more info : http://www.w3schools.com/xsl/xsl_examples.asp

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |