Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

USER_item_created - Edit an item with using post action

Experimenter
Experimenter

Hi,

 

I need a customization for an item type, so i create a dynamic link library to achive that with using post action (USER_item_created). I want to get the created item tag and do something on it, but the item tag and item revision tag returns NULL.

 

Here is the sample code..

 

extern int ITK_user_main(int argc, char * argv[])
{
     (CUSTOM_EXIT_ftn_t)CUSTOM_method_register_callbacks();

     return ITK_ok;
}

 

extern DLLAPI int CUSTOM_method_register_callbacks()
{
     CUSTOM_register_exit("CUSTOM_method", "USER_item_created", (CUSTOM_EXIT_ftn_t)CUSTOM_method_call);

     return (ITK_ok);
}

 

extern DLLAPI int CUSTOM_method_call(int *decision, va_list args)
{
     tag_t tItem = NULLTAG;

     tag_t tItemRev = NULLTAG;
     char * cItemID = va_arg(args, char *);
     char * cItemRev = va_arg(args, char *);

     printf("Item ID: %s\n", cItemID); // Item ID gets correctly
     printf("Item Revision : %s\n", cItemRev); // Item Revision gets correctly

 

     ITEM_find_item(cItemID, &tItem); // Item Tag is NULL ?

     ITEM_find_revision(cItemID, cItemRev, &tItemRev); // Item Revision Tag is NULL ?

 

     if (tItem != NULLTAG)
     {
     *decision = ONLY_CURRENT_CUSTOMIZATION;
     }
     else
     {
     *decision = NO_CUSTOMIZATION;
     }
     return ITK_ok;
}

 

Best regards.

4 REPLIES 4

Re: USER_item_created - Edit an item with using post action

Do you want to just add a post action on item creation? or is there any special requirement which can be fulfilled by user exits?

 

can you explain the requirement?

 

 

Re: USER_item_created - Edit an item with using post action

Experimenter
Experimenter

I will create some dataset after creating new item revision (data will come other system) and some changes on item revision relations. I research doing all that on post action, but it requires custom codes on BMIDE. So I want to try USER libs. According to the documentation it sould be possible.

 

In documentation it says:

 

USER_EXITS_API int USER_item_created ( const char * item_id, const char * revision_id )

 

This USER EXIT ITK provides a hook point for customers to plug the customization codes into the item creation. It is called at the end of successful item creation.

 

Parameters

item_id (I) Id assigned to newly created item

revision_id (I) Revision id assigned to the newly created item revision

Re: USER_item_created - Edit an item with using post action

try this, without writing single line you can do it.. if only need to is to create dataset upon item creation

 

Capture1.PNG

 

 

Capture2.PNG

Re: USER_item_created - Edit an item with using post action

Experimenter
Experimenter

We already use createObjects extension for some customizations, but I need dll for some reasons. We will start multiple process after item created. Thanks for your reply. I think we should learn how to write custom codes on BMIDE.