01-29-2018 05:41 AM
Hi everybody,
I found unfortunaly nothing about my error in GTAC or in this forum.
My goal: Create a new volume into a new FSC Server
Perhaps, one thing miss into the fmsmaster ? (*nameofserver is changed manually for this post)
<fscgroup id="CZMFSC"> <fsc id="FSC_CZMS_TCTST_FSC1" address="http://nameofserver:4544" ismaster="false" /> </fscgroup>
Thank you
Solved! Go to Solution.
01-29-2018 10:25 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
01-29-2018 11:36 AM
Hi RandyEllsworth,
thank you for your help. I've do that, the problem is... Firewall of the server.
I need to open the correct port.
But thank you for your help.
03-14-2018 02:58 AM
Hi,
You can install the New FSC server, once it is installed then you can add the details for new FSC in the master FSC file and restart the Master and client FSC services.
once it is implemented open TC and select the option in organization to create new volume.
Provide the details for Node Name, FSC ID , Volume name and also the details for the directory where u want to store the volume.
once the input is given, you can create a new volume and details will be written in the master fsc file.
you can restart the FSC if the Master configuration file is not same on server and client machine.