Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to create new revision for CATdrawing part in teamcenter 10

Experimenter
Experimenter

While we try to create new revision it thows following erros(attached)

 

unable to create new item revision 

"No additional object type "CATDrawing can be attached with a relation 'Match All' under the object XXXXX of type "Item Revision" because this would exeed the set limit for the primary object.Please refer the rule for "Item Revision,CATDrawing,Match all"

 

but we are having issue with specific drawing part  xxxxx only.Other parts with same object type can be revised without any issue 

 

I have attached Syslog as well 

 

Can anyone help me to revise this drawing part ?

 

Thank in advace 

2 REPLIES

Re: Unable to create new revision for CATdrawing part in teamcenter 10

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

When you try to revise it, if you look at the "Define Attached Data" step do you see the CATDrawing set to Copy as Reference? My guess is that the GRM rule for Item Revision -> CATDrawing is one to many, and copying the existing CATDrawing to the new IR as a reference, i.e., creating link from the CATDrawing under the orginal IR to the new IR, breaks the primary object's (the IR) cardinality rule.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Unable to create new revision for CATdrawing part in teamcenter 10

Builder
Builder
perhaps you GRM rule on your revision is set to 1, try release the dataset/revision and revise. if works, it is your GRM rule.