Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to install TcExcelAddin : Exception reading manifest from file [...]

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi everyone,

 

I installed the office integration and I cannot make it work for Excel.

It's working fine for word.

 

When trying add the Teamcenter add-in, I have an error : Exception reading manifest from file C:/Siemens/TC_ROOT/Office%20Client/TcExcelAddin.vsto: the manifest may not be valied or the file could not be opened.

 

I found online that it could be related to .NET Framework but I tried with 4.0, 4.5 and 4.5.2 and it didn't work. (When installinf the integration it is written that the requirement is 4.0)

 

Does anyone as an idea of what could be the problem here ?

 

PS: See the error in the attachment.

 

Thank you in advance

 

Sènan

4 REPLIES 4

Re: Unable to install TcExcelAddin : Exception reading manifest from file [...]

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

This issue was linked to ther version of .net framework. I had to installed .net framework 4.5.1 to solved the issue.

Re: Unable to install TcExcelAddin : Exception reading manifest from file [...]

Creator
Creator

There are prerequisites listed below to be installed before office integration.

 

o2007pia

vjredist64

vstor_redist

vstor40_x64

 

Re: Unable to install TcExcelAddin : Exception reading manifest from file [...]

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

In my way to solve the issue, I checked the prerequisite.

But as said above, the issue was only coming from the version of .net framework installed.

Highlighted

Re: Unable to install TcExcelAddin : Exception reading manifest from file [...]

Creator
Creator

Try by installing .NET Framework 4.5.1 Multi-Targetting Pack