Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to open dataset: No compatible tool is found.

Experimenter
Experimenter

Good morning everyone,

i have a problem with a custom dataset and his custom tool.

I had created a custom Dataset to work with a GantProject file into Teamcenter and i created the custom Tool for have a possibility to oper this file with Teamcenter.

I configured the tool in this mode:

MIME/TYPE: application/x-ganttprojent (i used the free tool filetypesman to founf the specific mimetype but without result so i do a search in Google and i found this)

Shell/Symbol: %TC_BIN%/run_gant.bat where into this file i write the *.exe file of application

Input and Output file valued with BINARY

Win Launch Command: "C:\GanttProject\ganttproject.exe" (the last test that i do)

I configured the gant dataset in this mode:

Tool for Edit\View: ABC4_GANT

References :*.gan, *.GAN

Tool Action: ABC4_GANT for Open,OpenUsing,Print, PrintUsing with export references. I try to set parameters but without result.

 

When i try to open dataset doesn't work: i see into RACfile and i find this error:

WARN 2017-03-09 09:54:23,968 - Windows Server 2012 R2 () - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment (1.8.0_51-b16) - 3.8.0.v20120529-1548
WARN 2017-03-09 09:54:34,938 - FCC Interface initialized in 8 ms.
ERROR 2017-03-09 09:54:48,579 - Unable to open dataset: No compatible tool is found.
Unable to open dataset: No compatible tool is found.
at com.teamcenter.rac.kernel.AEShell.done(Unknown Source)
at org.eclipse.core.internal.jobs.JobListeners$3.notify(JobListeners.java:39)
at org.eclipse.core.internal.jobs.JobListeners.doNotify(JobListeners.java:112)
at org.eclipse.core.internal.jobs.JobListeners.done(JobListeners.java:152)
at org.eclipse.core.internal.jobs.JobManager.endJob(JobManager.java:647)
at org.eclipse.core.internal.jobs.WorkerPool.endJob(WorkerPool.java:105)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:71)

 

 

I thought to set up the bat file like this:

set GANT_PATH=""C:\GanttProject\ganttproject.exe"

%GANT_PATH% %1

but i don't know which parameters i have set.

 

Can you help me to solve this problem? I tryed to use diffent BMIDE configuration but without good result.

 

Thank you very much,

have a nice day everyone.

 

Francesco

 

 

 

 

 

 

3 REPLIES

Re: Unable to open dataset: No compatible tool is found.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

 

Is there a system level file association for these extensions: *.gan, *.GAN?

 

If there is a need, you may want to configure TC to avoid using default viewer for the above extensions. 

 

Best Regards

Harish

Re: Unable to open dataset: No compatible tool is found.

Experimenter
Experimenter

Hi Harish,

thank you very much for your response.

There is a system level file for this extension (I attach 2 image).

For "using default viewer" you mean to associate the "PV" tool to the dataset? How can I configure it?

 

I'm banging my head in this problem for days Smiley Sad

 

Thank you,

Francesco

Re: Unable to open dataset: No compatible tool is found.

Valued Contributor
Valued Contributor

@francesco_t3d,

 

Were you able to resolve this issue?  I am experiencing a similar issue with a custom dataset.

 

Looking forward to your response.

 

Thanks, 

Jake