Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to run backup_xmlinfo.exe

Hi friends,

 

I am getting POM_INIT_Module error when i attempted to rum backup_xmlinfo.exe.

 

Can anybody give suggestion to solve this problem

 

Thanks in advance

2 REPLIES

Re: Unable to run backup_xmlinfo.exe

Legend
Legend

Error 515194 says: The TC_DB_CONNECT information is not set.

 

Did you run tc_profilevars?

---

Thanks and Regards

Yogesh Fegade

Re: Unable to run backup_xmlinfo.exe

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

Yogesh has it right. You did not run backup_xmlinfo in a Teamcenter command window. Your environment is not set. To run in a normal command window you'll need to:

set TC_ROOT=<path_to_tcroot>
set TC_DATA=<path_to_tcdata>
call %TC_DATA%\tc_profilevars.bat

 

Note: Its better to use a mapped drive than a UNC path for TC_DATA. Batch scripts don't like UNC paths.

 

Next, validate that your environment is set correctly...

set T

Note: You should see a bunch of Teamcenter environment variables listed.

 

 

Then you can run a Teamcenter utility.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4