Cancel
Showing results for 
Search instead for 
Did you mean: 

Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Valued Contributor
Valued Contributor

Hi All,

 

I'm using T4EA to import data into Teamcenter from a legacy database.

 

The approach I'm using is the following:

In a scheduled job I'm reading the legacy database, and based on the changes happened there I'm creating some T4EA Batch Jobs, that are intended to update some items in Teamcenter.

 

It's not uncommon that I have in one scheduled job more than 1 million SQL statements executed in the legacy database.

If there are a lot of changes in the legacy database, (that implies even more SQL statement executions) than at a certain time I get the following error: 

 

LAST ERROR MESSAGE :: (TCL ERROR ON PIPE SERVER)
 java exeption function=staticRun in class=de/tesis/plmware/objects/commands/WithCommand
    while executing
"tpco_sendECMD $handle $timeout $command $quotedArgs"
    (procedure "::T4X::JAVASERVER::sExecute" line 14)
    invoked from within
"::T4X::JAVASERVER::sExecute 514 with 514.*23651 executeQuery"
    ("eval" body line 1)
    invoked from within
"eval ::T4X::JAVASERVER::sExecute $serverHandle with $handle $methodName $args"
    (procedure "T4X::OBJECTS::tplet" line 17)

 

Could someone help me how could I find out what's the root cause of this?

 

Regards,

Csaba

Software Engineer
7 REPLIES 7

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

 

Did you check the gateway logs by setting the trace level to the lowest value (I think to 'info'?!)

what do those logs say?

 

Can you share the log statements preceding the error statement?

 

Harish

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Valued Contributor
Valued Contributor
Hi Harish,

I'm really glad that you've replied. :)
Unfortunately I'm quite new in this T4x/T4EA word, so a lot of things are not clear for me.

In the T4EA documentation I couldn't find where to set the log level. Could you give me a hint for this?

Regarding the logs... there are quite a lot of them (user logs, session logs, system logs, and the log for my script). And unfortunately I couldn't find anything relevant in them... :(
Could you give me a hint in which one I should get a closer look?

Br,
Csaba
Software Engineer

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Csaba,

 

I'm trying to configure T4EA for similar kind of requirement. I need to integrate TC with one of the legacy system using T4EA. Could you please share the steps I need to follow in order to connect GS to legacy system using odbc or jdbc or anything.

My pretty new in T4EA.

Appreciate your help!

 

Regards,

Ankush Manhotra

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Valued Contributor
Valued Contributor

@ZsCsaba Looks like pipe is timing out. Just add the below lines in the begining of your script. You can change the timeout value in sec (current value 7200s) as per your preference.

 

# Sets timeout interval.
set MaxRuntimeInSecs 7200 ;# in seconds
set ::qcmdet [expr { [clock seconds] + $MaxRuntimeInSecs }]

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Experimenter
Experimenter

Hi,

Currently we are facing same error. Any luck after changing timeout?

Regards,

Hari Vamsi

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Valued Contributor
Valued Contributor
Hi,

No luck from our side. But we have read in one of the documentations that this is not a real error. Of course, it generates us a lot of problem, but if Siemens said so... it's not an error. We have to live with it...
Software Engineer

Re: Unidentifiable T4EA error: TCL ERROR ON PIPE SERVER

Experimenter
Experimenter
Hi,
I found out the reason for us. It was because of using wrong version of sap libraries

Regards,
Hari Vamsi
http://www.plmcadutilities.com