07-22-2018 03:41 PM
Hello everyone,
I have a weird behavior with the integration Office.
Indeed when I double click on an Office dataset, this one seems to check out in Teamcenter, however in Offices it does not seem it, the icons are not all activated and the mapped properties are not synchronized.Befor doble click
After doble click
In OfficeWhen I try in office with "open and check out" directly on the dataset, I have access to all the icons in officeand properties are synchronized.
How could I have this behavior on double-click ?
Best regards,
Solved! Go to Solution.
07-23-2018 10:08 AM
Hi Ben,
I'd be interested to see a solution for this also.
I believe this is quite a well known issue with the intergration.
I have atually now adviced people to only open through the MS application as we where also finding that when opened through Teamcenter the document was being saved to a temp location and not back to Teamcenter.
Thanks Matt
07-23-2018 10:39 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
07-23-2018 11:16 AM
Good afternoon, I also encountered this when I tested the mechanism for creating Markup in MS Word with the integration of Teamcenter, so that it worked correctly you need to open the document from Word using the Teamcenter tab, otherwise Markup does not work normally. Most likely this is how the integration with MS Office works. Moreover, it causes problems if you use several rich clients. To open a MS Word document from Teamcenter, you need FCC, and hence the FMS_HOME environment variable, and it reads the environment variable of your computer's parameters. When you use several rich clients, you usually set FMS_HOME when you run a rich client. But MS Word with Teamcenter integration works separately from a rich client (it does not read FMS_HOME, which is set when the rich client starts up). I have so far found a way out, this is to create two shortcuts for MS Word each with its FMS_HOME and I do not really like it.