Cancel
Showing results for 
Search instead for 
Did you mean: 

Update TC10 - removing Dispatcher Services?

Builder
Builder

Hi,

 

I want to Update Teamcenter 10.1.2 to TC10.1.6.1. In the Administration Documentation I can read:

 

If your configuration includes Dispatcher Server, remove Dispatcher services
(scheduler, module, Dispatcher client) before installing patches.

 

Do they really mean "remove" the services or only stopping?

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12
4 REPLIES

Re: Update TC10 - removing Dispatcher Services?

Esteemed Contributor
Esteemed Contributor

They really mean remove, they must be re-installed afterwards anyways to get them updated.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Update TC10 - removing Dispatcher Services?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

If you're on the Windows platform, you can remove a service using:

 

sc delete <service_name>

on a command line. Run this command to get the service's name for the above command:

 

sc query | more

 

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Update TC10 - removing Dispatcher Services?

Esteemed Contributor
Esteemed Contributor

The dispatcher services are best managed through the batch script shipping in the BIN folder of the dispatcher installation Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Update TC10 - removing Dispatcher Services?

Builder
Builder

Yes, I have used this tool in the bin folder. It works fine, except one of the 3 services - the DispatcherClient has for some reason a different version name, than the other 2. I have to change the batch in one row, so that it points to the right name (and version) of the service. Then it works too.

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12