Cancel
Showing results for 
Search instead for 
Did you mean: 

Update dft and PDF generation after workflow validation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

When validating an item (SEpart+SEdraft), the workflow write the validation date in a custom property

Récuperation d'info dans propriété custo.png

 

 

this property is mapped with SE and put in a cartouche. I’m using SEEC_Workflow_PDF_Generation.exe, the Define_SolidEdge_Properties_ForWorkflow_ToSync.ini and the handler TCRS-export-signoff-data

TCRS-export-signoff-data.png

 

My questions are :

• How to configure the Define_SolidEdge_Properties_ForWorkflow_ToSync.ini to be able to put the custom property in the PDF ?

 

• In my test workflow, the PDF is correctly generated and with the standard properties

PDF à jour.png

 

 

, the plan .dft is up to date but the picture of the dft in the viewer isn’t

Image dft pas à jour.png

 

 

, how can I make for it to be automatically updated as well ?

 

 

Thank you in advanced for your answers.

2 REPLIES

Re: Update dft and PDF generation after workflow validation

Genius
Genius

Hello,

 

Whot version TC and SE you have ?

In a past checked this tool but didnt work. I had information from GTAC that isnt working witch TC 10.1.

SE ST9 + TC 10.1.7

Re: Update dft and PDF generation after workflow validation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

Sorry for the long absence.
I'm using TC 10.1.5 and Solid Edge ST9

The most important problem here is the no update of the image:
I just tried now and i can see that on the released ItemRevision

the .emf and the .qaf are not updatedthe .emf and the .qaf are not updated

 

Best regards,