Cancel
Showing results for 
Search instead for 
Did you mean: 

Upgrading BMIDE templates from 8.3

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello forum,

 

I am triyng to upgrade a test environment for a client from Temcenter 8.3 to TC 12. I have understood that I have to go through several versions so that is the plan.

What I need for that is to upgrade the BMIDE customization templates before upgradeing the server because TEM is askingfor them during the server upgarade process.

The issue is that I do not have the original BMIDE projects. I only have the TC_Home and TCDATA directories.

I know that in the tcdata/model/ folder the templates are stored but they are not the BMIDE projects.

The quiestion is how can I upgrade from 8.3 with the template only from the tcdata/model/ folder.

 

Thanks for the help!

2 REPLIES 2

Re: Upgrading BMIDE templates from 8.3

Gears Phenom Gears Phenom
Gears Phenom

Re: Upgrading BMIDE templates from 8.3

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks for the reply.

I tried the solution in the linked topic but it didn't work. Of course it is also possible that I missed something but I followed the tips to my best knowledge.