Cancel
Showing results for 
Search instead for 
Did you mean: 

Use EPM-assign-responsible-party-dynamic participant to set Issue Owner

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

I wish to assign a Participant to the Issue Owner at the very beginning of a workflow.

 

See attachment for screen shots.

I'm pretty sure BMIDE C2_IssueOwner Participant is pointing to the correct Issue type.

 

I think I am doing this correctly but I am getting the following error.

 

The operation has failed, because the participant type could not be retrieved from the keyword "$ISSUE_OWNER".
Action handler 'EPM-assign-responsible-party-dynamic-participant' on action 'Start' in task 'Set Issue Owner' recorded the following 1 entries.
The initial action was successful, but a subsequent task in the workflow may have failed. For additional details, please read the rest of the error messages.

 

 

Any ideas as to why this is failing?

Thanks 

 

1 REPLY 1

Re: Use EPM-assign-responsible-party-dynamic participant to set Issue Owner

Gears Phenom Gears Phenom
Gears Phenom

Hello, you can make a screenshot, how do you use the arguments of the EPM-assign-responsible-party-dynamic handler? I think they should look like this:

 

-name=ISSUE_OWNER
-assignee=user:user