Cancel
Showing results for 
Search instead for 
Did you mean: 

Using the tcradmin command line function

Pioneer
Pioneer

Has anybody used the tcradmin command line function in TcSE?

I can set it to process a single object using the -selected option but fow do i set it to process 2 onjects? THe API reference says use a comma separated list but:

 -selected139.0.131273186,139.0.131274100 only processes the first item, as does

 -selected139.0.131273186, 139.0.131274100

 

Do I need to put my list in braces, brackets, single quortes, double quotes .....?

 

Any help gratefully received

Mark