Cancel
Showing results for 
Search instead for 
Did you mean: 

VMWare ESXi compatibility with TC 11.x

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

The hardware/software compatibility matrix says ESXi 5.5 is certified for 11.x, I take it this means ESXi 5.5 is certified for  all versions from 11.0 to 11.3?

 

Thank you.

2 REPLIES

Re: VMWare ESXi compatibility with TC 11.x

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Yes. And Hyper-V is certified for Tc11.3. Really they certify the OS and not actually the VM software.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: VMWare ESXi compatibility with TC 11.x

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Thanks for the speedy reply, Randy. Also, if one were to have ESXi 6.5 I guess one would have to be running/upgrade to TC 11.2.1 for it to be "officially certified" for production use? Just trying to understand the wording and implications of the compatibility matrix.