Cancel
Showing results for 
Search instead for 
Did you mean: 

Viewing STP files in embedded viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

Is it possible to view STP files in the embedded viewer in Teamcenter?

 

Cem

24 REPLIES 24

Re: Viewing STP files in embedded viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you using TC-NX integration?

How are you adding the STP files to the item revision in Teamcenter, as a separate dataset?

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Viewing STP files in embedded viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Yes, Using TC-NX integration.
I can add STP directly using drag-drop without having UGMASTER or JT data.

Cem ALPAY
Üçgen Yazılım Ltd. Şti.

--Mobil cihazımdan gönderildi--
--------------------------------

Re: Viewing STP files in embedded viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

I am certain about the DXF,DWG,UGMASTER,UGAPRT,PDF preview, but not about STP (or STEP).

 

When you import some dataset in TC, option 'Tool Used' shows the tool for that particular dataset.

UGMASTER/UGPART - UGII V10-BASE

Bitmap - PV

Word file - MSWord

PDF - PDF-Tool etc.

 

I am wondering the tool to be used (if it is available) to import it directly. In my case when I import it using 'Ctrl+D' > Select the STP file from OS location, it's showing tool used as 'CAE_Dummy' which seems to be incorrect.

 

If I drag and drop STP file to item revision, it does get added. When checked under named reference there is nothing to show, it's empty. Can you check the same? I am doubtful about the preview of the STP file format in TC.

 

EDIT: Preferences need to set for the dataset to view in the viewer

 defaultViewerConfig.VIEWERCONFIG
<dataset type>.<viewer type>=<list of named references>

For example, to show PDF, UGMASTER and UGPART datasets the following preferences can be used

PDF.TCTwoDViewer=PDF_Reference,PDF
UGMASTER.DirectModelViewer=UGPART
UGPART.TCTwoDViewer=UGPART

 

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Viewing STP files in embedded viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

How is it possible to make STP file read by the TCViewer?

Re: Viewing STP files in embedded viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

You have TC-NX integration. Import STP file in NX part file and save it in Teamcenter as UGMASTER dataset.

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Viewing STP files in embedded viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I already know that is possible.
I was wondering if STP files could be directly visible through the Viewer or not.

Saygılarımla,

Cem ALPAY, Yönetici
ÜÇGEN YAZILIM LTD. ŞTİ.
TEL: 0216 550 52 06

[cid:image001.jpg@01D2B467.FA6A5730]

Re: Viewing STP files in embedded viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

I think answer is NO.

 

@BenBroad: Can you give your opinion about this?

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Viewing STP files in embedded viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I believe it is possible with JT-STEP translator.

Saygılarımla,

Cem ALPAY, Yönetici
ÜÇGEN YAZILIM LTD. ŞTİ.
TEL: 0216 550 52 06

[cid:image001.jpg@01D2B46B.D82A31F0]

Re: Viewing STP files in embedded viewer

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

STEP (*.stp or *.step) files are not supported for viewing in the embedded viewer in Teamcenter . With the correct TcVis license the STEP file can be opened in standalone TcVis.

 

Regards, Ben