Cancel
Showing results for 
Search instead for 
Did you mean: 

Visualization connect with Teamcenter

Genius
Genius

Hello all

 

I have a problem on Visualization connect with Teamcenter

I open AWC download file and use visualization will show this message

Even when I in Teamcenter click twice file  will open Visualization

It still wrong

擷取.PNG

 

Anyone know what's wrong with this?

 

Best regards

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10
2 REPLIES 2

Re: Visualization connect with Teamcenter

Hi, 

 

What is the file extension you trying to open?

Are you able to open native/standalone TC Visualisation?

Can you download named the reference to the Local system and then open in Visualisation?

 

 

Re: Visualization connect with Teamcenter

Genius
Genius

Hello Ganesh-IZ

 

File is vvi

YES, I can open TC Visualisation software

Use TC Visualisation login TC or login TC open file is working

But if I use AWC download file,then I can't open it

It show me that wrong message

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10