Cancel
Showing results for 
Search instead for 
Did you mean: 

Volume statistics missing after adding new volumes %full and free space Used and Free space

Pioneer
Pioneer

After adding two new volumes to Teamcenter the two new volumes don't display the statistics information. The exisiting volumes show the information popluated.

 

The new volumes are being written to succsessfully and all looks ok. With the second new volume set as failover in the preferences it is now writing data to both. The old volumes are in excess of 90% full hence the need to add more volumes.

 

 

1 REPLY 1

Re: Volume statistics missing after adding new volumes %full and free space Used and Free space

Pioneer
Pioneer

I figured out the problem when Teamcenter added the two new volumes it modified the fsc configeration files. The paths were:

 

\\\\<server>\volumeshare$

 

Once I edited the fsc master configuration files on all applicable servers to:

 

\\<server>\volumeshare$

 

Then restarted the fsc services the volume statisitics started to work.