Cancel
Showing results for 
Search instead for 
Did you mean: 

What are the feature differences between TC 11.2.3 on AWC 4.0 and TC 11.5 on AWC 4.0?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

What are the feature differences between TC 11.2.3 on AWC 4.0 and TC 11.5 on AWC 4.0?

 

Do I have to use TC 11.5 with AWC 4.0 for utilizing 100% of the functionality in Active Workspace. If I do not use 11.5 and use 11.2.3 what features will be lost?

 

Thanks,
Sanjay