Cancel
Showing results for 
Search instead for 
Did you mean: 

Why teamcenter 11 rapid start installation do not install the Teamcenter Integration for NX features

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Why teamcenter 11 rapid start installation do not install the Teamcenter Integration for NX features ?

2 REPLIES

Re: Why teamcenter 11 rapid start installation do not install the Teamcenter Integration for NX feat

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Because NX requires templates to be imported using nx_clone to maintain relationships. This requirement is also why it is hard to import legacy data into Teamcenter whenever NX is involved.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: Why teamcenter 11 rapid start installation do not install the Teamcenter Integration for NX feat

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks